Part Number: TMS320F28069
Other Parts Discussed in Thread: DRV8301,
Tool/software: Code Composer Studio
Connecting TMS320F28069 control card with DRV8301 , CCS shows error:
ne of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 7.0.100.0)
Why do I need to powerup DRV8301 then only ccs is able to detect TMS320F28069?
Is something from DRV8301 triggering TMS320F28069 so ccs can detect ftdi chip or xds100 emulator?