Part Number: LAUNCHXL-F28069M
Tool/software: Code Composer Studio
hi,all.
I have ask a question about the application of instaspin-foc.
http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/796645/2947434#2947434
but I still have some uncertainty about my application in instaspin.
please give me a help. thanks.
I still do not know how to calculate or estimate the motor wind Irms current according to the peak dc bus current 150A.
because I should use the motor Irms current to design my full current sensing scale .
the Irms is nothing to do with the Ibus in math?
or is there any design experience value between the Irms and the Ibus ?
the Irms = 2*Ibus or Irms = 3* Ibus ???
I wonder that whether the in-line current sensing is better than the shunt resistor current sensing method especially in current sensing precision ?
in my opinion,the peak current of in-line current sensing perhaps is bigger than the peak current of the low side shunt resistor current sensing method. so the full current scale in in-line mode is bigger than the shunt resistor .
in such a big current ,it is difficult to select a suitable Rshunt(value Ω and power W) in inline mode.
if I use the in-line current sensing with an AMC1301,whether I need to change the instaspin current sensing program.
because the instaspin use the shunt resistor current sensing method.
thanks.
all the best .