Part Number: TMS320F280049
Hi experts,
In F280049's block diagram, a trip zone is in the down stream of DB module. But, when I software force a trip event to let A and B of PWM3 to low with below dead band configuration (Marked signal connection in red line). The trip result is that A and B are complementary. I'd like to know if I am do anything wrong. (please see attached code)
BTW, could you help me check these two things. Firstly, If I am doing software trip in a advised way. Secondly, if there is a way to trip both A and B low in my PWM configuration.
Thanks
Dead band configuration:
PWM configuration:
EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up EPwm3Regs.TBPRD = PWM3_TIMER_MAX; EPwm3Regs.TBPHS.all = 0x00000000; EPwm3Regs.CMPA.bit.CMPA = PWM3_TIMER_MAX/2; EPwm3Regs.AQCTLA.bit.CAU = AQ_CLEAR; EPwm3Regs.AQCTLA.bit.ZRO = AQ_SET; EPwm3Regs.AQCTLB.bit.CAU = AQ_SET; EPwm3Regs.AQCTLB.bit.ZRO = AQ_CLEAR; // Dead band EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL; EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; EPwm3Regs.DBRED.all = DEAD_BAND; EPwm3Regs.DBFED.all = DEAD_BAND; // // TBCLK = SYSCLKOUT // EPwm3Regs.TBCTL.bit.HSPCLKDIV = 1; EPwm3Regs.TBCTL.bit.CLKDIV = 0; EPwm3TimerDirection = EPWM_TIMER_UP; EALLOW; CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS;
Software force tripping configuration:
if(i == 1){
EPwm3Regs.AQSFRC.bit.ACTSFA = 1; // Action When One-Time Software Force A Is Invoked: Clear
EPwm3Regs.AQSFRC.bit.ACTSFB = 1;
EPwm3Regs.AQSFRC.bit.OTSFA = 1; // Initiates a single software forced event
EPwm3Regs.AQSFRC.bit.OTSFB = 1;
EPwm3Regs.AQCSFRC.bit.CSFA = 1; // Force low on A output
EPwm3Regs.AQCSFRC.bit.CSFB = 1; // Force low on B output
}
Sheldon