Other Parts Discussed in Thread: TIDM-1001
Hi,
Customer is doing a power module:
- Input: 88V-264V Vac or Vdc.
- First Stage: boost PFC, output 400V VDC
- 2nd Stage: half-bridge LLC, output 48V Vdc/20A
- Another requirements: 97% efficiency, parallel connect the power modules(up to 4-5 modules)
They are asking, if we have current balancing support, hardware or software solution.
Thanks a lot.
Br, Jordan