This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using F2806X ISO-CONTROLCARD [R0.4] with USBDockingStation [R3], I am running BLDC motor of 60V, 250W attached with wheel for two wheeler application with sample code which is located here C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\BLDC_Sensored. I have my own driver card with driver IC IR2104S which is similar to DRV8312 as used in DRV8312EVM Rev D board. DFuncDesired is directly controlled by throttle.
with LEVEL4 it is working fine. I am able to control the speed. there is only one small issue when I applied throttle motor rotates initially in counter clockwise direction then it rotates in clockwise direction. I have already read documents regarding the sample code. what is the possible reason?
one more question how can I apply more torque initially, I mean by using which variable?