This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRINSPIN: TMDSHVMTRINSPIN

Part Number: TMDSHVMTRINSPIN

i have no issue to connect from the Card F28069M USB port , i see another port on the card i never been able to connect to it , and i was never able to connect to the HV kit using the USB built into the Kit mother board 

everytime it says VCP have issue i tried to i re install the USB driver in the device manger it do the same issue again 

  • The micro USB port on the right side of the F28069M controlCARD is for the host USB port on the device, not for JTAG debug connection. The mini USB port on the left is for XDS100v2 connection for debugging.

    You are recommended to use the USB port on the controlCARD for debugging, since it provides isolation as well as a secondary serial channel.

    If you wish to use debug connection on base board, please refer to the InfoSheet of the controlCARD for more information. Here is a part that talks about JTAG and UART connection selection.

    SW3: TRST/ ISO SCI communication signal enables
    Position 1 -
    ON - TRST signal from ISO JTAG circuit (USB connector J1) will be connected to F2806x. This configuration is necessary when using JTAG to debug the device and connect to Code Composer Studio.
    OFF - TRST signal from ISO JTAG circuit will NOT be connected to F2806x. This configuration is necessary when the application is running from flash at power up without debug capability.
    Position 2 -
    ON - The default option. SW3 in the “ON” position enables a UART COM link between the MCU and USB connector J1. This is accomplished using the FT2232’s USB-to-Serial port bridge and GPIO28 of the F28069 MCU.
    OFF - Disables the serial link between the MCU and USB connector J1. This allows GPIO28 to be used as desired by the baseboard that the controlCARD is plugged in to.