Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hello team,
my customer has the issue with initializing the CLA (getting ILLEGAL_ISR error), please find attached his CLA init function code based TI example and memory mapping.
Could you please advise if you can spot what he doing wrong, Thanks in advance
//###########################################################################
// Description:
//! \addtogroup f2806x_example_cla_list
//! <h1> ACOS Table-Lookup Algorithm</h1>
//!
//! This example implements a table lookup method of determining
//! the arccosine of a value.
//!
//! \b Watch \b Variables \n
//! - y - Accumulated results (angles in radians)
//
//###########################################################################
// $TI Release: F2806x C/C++ Header Files and Peripheral Examples V151 $
// $Release Date: February 2, 2016 $
// $Copyright: Copyright (C) 2011-2016 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#include "DSP28x_Project.h" // DSP28x Headerfile
#include "F2806x_Cla_defines.h"
// Include the test header file whose name is based on the test name
// which is defined by the macro TEST on the command line
#include "CLA_shared.h"
#define CLA_PROG_ENABLE 0x0001
#define CLARAM0_ENABLE 0x0010
#define CLARAM1_ENABLE 0x0020
#define CLARAM2_ENABLE 0x0040
#define CLA_RAM0CPUE 0x0100
#define CLA_RAM1CPUE 0x0200
#define CLA_RAM2CPUE 0x0400
#define HARDWARE 1
// Constants
#define OSCCLK (10000000UL) // < Internal OSC frequency
#define SYSCLK (80000000UL) // < System Clock frequency
#define PER_CLK_DIV (4) // < Low speed peripheral clock dividers
#define PER_CLK (SYSCLK/PER_CLK_DIV) // < Low speed peripheral clock
#define DIV_SEL (2) // < Clock divider selection
#define CLK_DIV ((SYSCLK * DIV_SEL)/OSCCLK) // < Clock divider
//CLA ISRs
__interrupt void cla1_task1_isr( void );
__interrupt void cla1_task2_isr( void );
__interrupt void cla1_task3_isr( void );
__interrupt void cla1_task4_isr( void );
__interrupt void cla1_task5_isr( void );
__interrupt void cla1_task6_isr( void );
__interrupt void cla1_task7_isr( void );
__interrupt void cla1_task8_isr( void );
// Main Function
void CLA_Init_Interrupts(void)
{
/* Assign user defined ISR to the PIE vector table */
EALLOW;
PieVectTable.CLA1_INT1 = &cla1_task1_isr;
PieVectTable.CLA1_INT2 = &cla1_task2_isr;
PieVectTable.CLA1_INT3 = &cla1_task3_isr;
PieVectTable.CLA1_INT4 = &cla1_task4_isr;
PieVectTable.CLA1_INT5 = &cla1_task5_isr;
PieVectTable.CLA1_INT6 = &cla1_task6_isr;
PieVectTable.CLA1_INT7 = &cla1_task7_isr;
PieVectTable.CLA1_INT8 = &cla1_task8_isr;
EDIS;
//Copy over the CLA code(if running in standalone mode from FLASH)
//memcpy(&Cla1funcsRunStart, &Cla1funcsLoadStart, (Uint32)&Cla1funcsLoadSize);
//Copy over the CLA math tables(if running in standalone mode from FLASH
//and using the CLAMath Library)
//memcpy(&Cla1mathTablesRunStart, &Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);
/* Compute all CLA task vectors */
EALLOW;
Cla1Regs.MVECT1 = (Uint16)((Uint32)&Cla1Task1 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT2 = (Uint16)((Uint32)&Cla1Task2 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT3 = (Uint16)((Uint32)&Cla1Task3 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT4 = (Uint16)((Uint32)&Cla1Task4 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT5 = (Uint16)((Uint32)&Cla1Task5 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT6 = (Uint16)((Uint32)&Cla1Task6 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT7 = (Uint16)((Uint32)&Cla1Task7 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT8 = (Uint16)((Uint32)&Cla1Task8 -(Uint32)&Cla1Prog_Start);
EDIS;
// Step 3 : Mapping CLA tasks
/* All tasks are enabled and will be started by an ePWM trigger
* Map CLA program memory to the CLA and enable software breakpoints
*/
EALLOW;
Cla1Regs.MPISRCSEL1.bit.PERINT1SEL = CLA_INT1_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT2SEL = CLA_INT2_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT3SEL = CLA_INT3_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT4SEL = CLA_INT4_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT5SEL = CLA_INT5_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT6SEL = CLA_INT6_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT7SEL = CLA_INT7_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT8SEL = CLA_INT8_NONE;
Cla1Regs.MIER.all = 0x00FF;
EDIS;
/* Enable CLA interrupts at the group and subgroup levels */
PieCtrlRegs.PIEIER11.all = 0xFFFF;
IER = (M_INT11 );
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
/* Switch the CLA program space to the CLA and enable software forcing
* Also switch over CLA data ram 0,1 and 2
* CAUTION: The RAMxCPUE bits can only be enabled by writing to the register
* and not the individual bit field. Furthermore, the status of these bitfields
* is not reflected in either the watch or register views - they always read as
* zeros. This is a known bug and the user is advised to test CPU accessibilty
* first before proceeding
*/
EALLOW;
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE|CLARAM0_ENABLE|CLARAM1_ENABLE|CLARAM2_ENABLE|CLA_RAM0CPUE|CLA_RAM1CPUE|CLA_RAM2CPUE;
Cla1Regs.MCTL.bit.IACKE = 1;
EDIS;
//--- Force one-time initialization Task 8 - zero delay buffer
Cla1Regs.MIER.all = 0x0080; // Enable CLA interrupt 8
asm(" IACK #0x0080"); // IACK - CLA task force instruction
asm(" RPT #3 || NOP"); // Wait at least 4 cycles
while(Cla1Regs.MIRUN.bit.INT8 == 1); // Loop until task completes
//--- Enable CLA task interrupts
Cla1Regs.MIER.all = 0x0001; // Enable CLA interrupt 1 (and disable interrupt 8)
asm(" EDIS"); // Disable EALLOW protected register access
//--- Enable the CLA interrupt
// PieCtrlRegs.PIEIER11.bit.INTx1 = 1; // Enable CLA Task1 in PIE group #11
// IER |= 0x0400; // Enable INT11 in IER to enable PIE group 11
// Enable INT11 in IER to enable PIE group 11
}
//###########################################################################
// CLA ISRs
//###########################################################################
__interrupt void cla1_task1_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task2_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task3_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task4_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task5_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task6_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task7_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
__interrupt void cla1_task8_isr( void)
{
ESTOP0;
PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}
Best regards,
Shai