Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Hi,
I'm using example code provided in the control suite "C2000Ware_1_00_06_00" for serial flash programming. I have configured GPIO84,GPIO85 for SCI boot mode. I ran serial_flash_programmer.exe with example "blinky_cpu01" and "F2837xS_usb_flash_kernels_cpu01" using the command
:> .\serial_flash_programmer.exe –d f2806x –k <~\f28069_flash_kernel.txt> -a <file> -p COM<num>
At the of programming I'm getting status code: VERIFY_ERROR (screenshot attached). What does this mean?