Hi,
There's a request on EMIF 1 on F2837x. 4 asynchronous devices are needed.
3 asynchronous devices are already connected to EMIF 1 by CS2/CS3/CS4. Another one is needed in the system. All of them are ADC. They don't want to use one CS2 to connect two devices by different address, as too much changes from the HW.
Can CS0 support it?
Thanks a lot.
Br, Jordan