Other Parts Discussed in Thread: UNIFLASH
This is with regards to the following thread:
When I go back to the device I had programmed before, I can verify the image without entering the CSM passcode. I am still curious why the hex file does not seem to work as well.
Summarizing:
1. The application requires the flash to be protected
2. The device does not program and or verify with a generated hex file via CCS
3. The programming and execution of the image works fine with a .out file, however the flash does not seem to be protected. I can verify the code without entering any passcode.
Could you please try to reproduce the issue on your end? You will not need any special code - the simplest blinky example is what I am using.
Thank you!