Part Number: TMS320F28027F
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE-DIGITALPOWER-SDK
Tool/software: TI C/C++ Compiler
Dear TI members,
I have a code that runs an ADC (4ch), and saves it in a buffer with function DLOG_4ch. I created my project based on the template project from TI in controlSUITE (C:\ti\controlSUITE\development_kits\TemplateProjects), and I have followed the instructions to implement the ADC_4ch and the DLOG_4ch based on the Digital Power Library Manual v3.5. I have been able to run this code, however there are 2 main questions that I haven't been able to find the answer yet:
1) How can I change the name of my .out file? Sometimes when there is an error, it shows "Project_name.out"
2) How I could call .c functions inside my ISR (which is written in ASM)? If I want to later implement my own .c functions that are not part of the DPlib library, would I necessarily need to write them in assembly? Because so far, every function in the digital power library being called is in .asm. The ISR code is attached below.
MY ISR Code:
;----------------------------------------------------------------------------------
; FILE: {3ph_pwm_acdc}-DPL-ISR.asm
;
; Description: {3ph_pwm_acdc}-DPL-ISR.asm contains the ISR for the system
; It also contains the initailization routine for all the macros
; being used in the system both for CLA and C28x macros
;
; Revision/ Version: See {3ph_pwm_acdc}-Main.c
;----------------------------------------------------------------------------------
;Gives peripheral addresses visibility in assembly
.cdecls C,LIST,"PeripheralHeaderIncludes.h"
;include C header file - sets INCR_BUILD etc.(used in conditional builds)
.cdecls C,NOLIST, "3ph_pwm_acdc-Settings.h"
;Include files for the Power Library Maco's being used by the system
.include "PWMDRV_1ch.asm"
.include "ADCDRV_4ch.asm"
.include "DLOG_4ch.asm"
;=============================================================================
; Digital Power library - Initailization Routine
;=============================================================================
; label to DP initialisation function
.def _DPL_Init
; dummy variable for pointer initialisation
ZeroNet .usect "ZeroNet_Section",2,1,1 ; output terminal 1
.text
_DPL_Init:
ZAPA
MOVL XAR0, #ZeroNet
MOVL *XAR0, ACC
; Initialize all the DP library macro used here
;---------------------------------------------------------
.if(INCR_BUILD = 1)
PWMDRV_1ch_INIT 1 ; PWM1A
.endif
;---------------------------------------------------------
ADCDRV_4ch_INIT 0,1,2,3 ; ADCDRV_4ch Initialization
DLOG_4ch_INIT 1 ; DLOG_4CH Initialization
LRETR
;-----------------------------------------------------------------------------------------
; Digital Power library - Interrupt Service Routine
.sect "ramfuncs"
; label to DP ISR Run function
.def _DPL_ISR
_DPL_ISR:
; full context save - push any unprotected registers onto stack
PUSH AR1H:AR0H
PUSH XAR2
PUSH XAR3
PUSH XAR4
PUSH XAR5
PUSH XAR6
PUSH XAR7
PUSH XT
SPM 0 ; set C28 mode
CLRC AMODE
CLRC PAGE0,OVM
; CLRC INTM ; clear interrupt mask - comment if ISR non-nestable
;-----------------------------------------------------------------------------------------
; call DP library modules
;---------------------------------------------------------
.if(INCR_BUILD = 1)
PWMDRV_1ch 1 ; PWM1A
.endif
;----------------------------------------------------------
ADCDRV_4ch 0,1,2,3 ; Run ADCDRV_4ch
DLOG_4ch 1 ; Run the DLOG_4CH Macro
;-----------------------------------------------------------------------------------------
; Interrupt management before exit
.if(EPWMn_DPL_ISR=1)
.if(EPWM1)
MOVW DP,#_EPwm1Regs.ETCLR
MOV @_EPwm1Regs.ETCLR,#0x01 ; Clear EPWM1 Int flag
.endif ; EPWM1
.if(EPWM2)
MOVW DP,#_EPwm2Regs.ETCLR
MOV @_EPwm2Regs.ETCLR,#0x01 ; Clear EPWM2 Int flag
.endif ; EPWM2
.if(EPWM3)
MOVW DP,#_EPwm3Regs.ETCLR
MOV @_EPwm3Regs.ETCLR,#0x01 ; Clear EPWM3 Int flag
.endif ; EPWM3
.if(EPWM4)
MOVW DP,#_EPwm4Regs.ETCLR
MOV @_EPwm4Regs.ETCLR,#0x01 ; Clear EPWM4 Int flag
.endif ; EPWM4
.if(EPWM5)
MOVW DP,#_EPwm5Regs.ETCLR
MOV @_EPwm5Regs.ETCLR,#0x01 ; Clear EPWM5 Int flag
.endif ; EPWM5
.if(EPWM6)
MOVW DP,#_EPwm6Regs.ETCLR
MOV @_EPwm6Regs.ETCLR,#0x01 ; Clear EPWM6 Int flag
.endif ; EPWM6
MOVW DP,#_PieCtrlRegs.PIEACK ; Acknowledge PIE interrupt Group 3
MOV @_PieCtrlRegs.PIEACK, #0x4
.endif ; EPWMn_ISR
.if(ADC_DPL_ISR=1)
; Case where ISR is triggered by ADC
MOVW DP,#_AdcRegs.ADCINTFLGCLR
MOV @_AdcRegs.ADCINTFLGCLR,#0x01 ; Clear ADCINT1 Flag
MOVW DP,#_PieCtrlRegs.PIEACK ; Acknowledge PIE interrupt Group 1
MOV @_PieCtrlRegs.PIEACK,#0x1
.endif
;-----------------------------------------------------------------------------------------
; full context restore
; SETC INTM ; set INTM to protect context restore
POP XT
POP XAR7
POP XAR6
POP XAR5
POP XAR4
POP XAR3
POP XAR2
POP AR1H:AR0H
IRET ; return from interrupt
.end
; end of file
Picture of the project's files: