Part Number: TMS320F28376D
Tool/software: Code Composer Studio
Hi Everybody ,
I have being using since long time CCS. 8.0.0.00016 + blackhawk NO problem at all .
now newer boards mounting same F28376D , using same PC , same CCS. 8.0.0.00016 and same blackhawk I cannot enter debug --> I get this error :
“C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_CPU1: File Loader: Verification failed: Values at address 0x93138@Program do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\Work\............\TMS320F28376D_cpu1\Debug\TMS320F28376D_cpu1.out: a data verification error occurred, file load failed.”
same newer board with newer DSP using another PC with CCS 8.3 and same Blackhwak are working . ( only thing we were forces to change in CCS8.3 was to change to lib rts2800_fpu32.lib to stop a compiling issue ) .
I tested same boards
using XDS100 exactly same behaviour
please what can be wrong ? due to legacy I must stay on CCS. 8.0.0.00016
in attach you have pictures of older ( working ) and newer ( NOT working ) F28376D devices using CCS. 8.0.0.00016 .
best regards
Carlo