This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT: Evaluation Kit Capabilities a External DC Power Supply

Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: TIDA-01606

In conjunction with operational testing of my three phase BLDC servo motors, I have the need to load test this motor which requires up to 13.5 Amps for a brief period (approx. 30 seconds to 1 minute in duration). My Question is; If I connect a External Isolating DC Power Supply with a max output rating of 350 VDC and 17 Amps, can I perform the load test up to 13.5 Amps with this TI Drive/Eval. Kit?

Ron Stewart