Part Number: TMS320F28069F
Other Parts Discussed in Thread: DRV8301, MOTORWARE
Dear team:
TI device: DRV8301-HC-EVM Rev D.
Routine: \...\sw\solutions\instaspin_foc\boards\drv8301kit_revD\f28x\f2806xF\projects\ccs5\proj_lab10a
The torque of EVM can reach 50H. Cm in normal test, But in the process of actual use, the user thinks that the torque of our product is too small. When the load is mutated (largen), The stability of this kit will be insufficient, and the actual output will be less than 50n.cm of torque, About 10 h.cm smaller. (Compare with a product in Germany which is the same as ours.)
Ask TI's engineers to provide solutions of weak and soft torque output at 300rpm of the motor. Thank you very much.
Best regards