Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Dear TI Hello,
I am working on a serial communication between my computer and the C2000 launchPad XL,
I am using the TI example usb_dev_serial_cpu0, I am connecting my serial communication device the GPIO18/19(SCITXDB/SCIRXDB) using 4 wires(TX,RX,GND,5V),
In the original code provided by TI, SCIA is used, In my application i want to use the SCIB,
I changed the code to be able to use the UARTB, but still can't communicate with my host application,
#define USB_UART_BASE UARTB_BASE //UARTA_BASE
#define USB_UART_PERIPH SYSCTL_PERIPH_SCI2 //SYSCTL_PERIPH_SCI1
#define USB_UART_INT INT_SCIRXINTB //INT_SCIRXINTA
EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 2; //SCITXDB
GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0;
GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3;
GpioCtrlRegs.GPADIR.bit.GPIO18 = 1;
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 2; //SCIRXDB
GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO19 = 0;
EDIS;
Thank you in advance,
S.Tarik