This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: Reprogram Z1-BOOTCTRL (for use Z2-BOOTCTRL)

Part Number: TMS320F28377D


Tool/software: Code Composer Studio

Hello,

I have a promblem to reflash Z1-BOOTCTRL. The pin of DSP is probably dead. So I want to use another boot pin with the Z2-BOOTCTRL but I can't reprogram the Z1-BOOTCTRL to set EMU_KEY to 0x00. But it is impossible to reprogram Z1, Z2-BOOTCTRL has been programmed.

How do I get past this security issue?

Thanks,

Paul

My error :

C28xx_CPU1: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: Please make sure the memory location you are programming have not already been programmed.
C28xx_CPU1: Error encountered during security operation. Operation Cancelled.