Part Number: TMS320F28069M
Hi,
we had a couple questions on the CAN Flash Kernel for the F2806x which is in C2000 Ware.
[] There are calls to F2806x Flash operations to erase and write. During these Flash operations, do interrupts need to be disabled, i.e. do these operations need to be atomic?
[] The CAN flash kernel does not have a checksum like the SCI flash kernel. In order for the CAN flash kernel to be reliable, an acknowledge message needs to go back to the CAN Host, to hold it off to send more CAN message until certain operations in the Flash kernel completed. In the SCI flash kernel, the checksum was used as an indirect ack to hold off writing a new block of data until the previous block as fully been written to flash. Can this be fixed on our side?
Regards,
--Gunter