Why we have 50-kΩ pulldown resistor on these pins?
Any attention needed when designing the circuit for these pins?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Why we have 50-kΩ pulldown resistor on these pins?
Any attention needed when designing the circuit for these pins?
Hi Howard,
This is due to the legacy design of the DAC channels that are internally connected to the ADC channels. There was not an option then to isolate these loads through mux switches. When designing circuits for these pins, specifically when these are used as ADC inputs, ensure that the source impedance of the circuits feeding to these inputs are low (in tens to low hundreds of ohms) so that signals will not be severely attenuated. If source impedance cannot be reduced, consider adding buffers prior to driving these channels.
Best regards,
Joseph