Part Number: TMDSDOCK28335
Tool/software: Code Composer Studio
Hello,
I am using a f28335 control card with docking station. I was trying to do sci communication. Suddenly I started getting error 1156 (Low Power mode ) and sometimes Error 1041( Debug Probe) while launching debug. I tried many things like restarting CCS and Laptop but same error persisted. After that I changed the SW1 position on control card to ON and suddenly I was able to connect and debug the flash program. But after 2-3 times I got the same error while debugging. Again I made SW1 ON-OFF and it worked. After sometime it again failed. I dont know why this trange behavior is happening. I guess my board is fine because due to error I was unable to connect to the board through JTAG but my previous program was running from flash. I checked all the voltage levels and everything seems fine. So can anyone suggest or guess what's happening exactly? Is it laptop problem or docking station FTDI chip problem or Control Card problem ? I don't know but some time I felt that whenever I added one statement of "SPRINTF" in my code that error happend. There is no logic but may be a coincidence. Sometimes the debug or jtag part gets disconnected while running also.
Thanks in Advance
Suraj