Hi Everyone
I need more than 12 ePWM signals for my applications using the mentioned controller for which I am thinking of synchronising PWMs of two DSPs together. Can anyone suggest how to do it ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Everyone
I need more than 12 ePWM signals for my applications using the mentioned controller for which I am thinking of synchronising PWMs of two DSPs together. Can anyone suggest how to do it ?
Mahetab,
this is relatively common, you can use the sync in and sync out funcitons of the PWM. Please see this post here for more details: https://e2e.ti.com/support/microcontrollers/c2000/f/171/p/612493/2261541#2261541 .
Please note when doing this there is a small additional delay in the sync chain that you will need to compensate for, this is described in both datasheet and the following post.
http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/22613/86678#86678
Regards,
Cody
Hi,
Also note that some of our newer devices, such as the F2837x (F2837*D/F2837*S), have more ePWM modules than the F28335 device. As a result, they can output more PWM waveforms - without needing to utilize multiple devices. These newer devices would also have more features.
If you have sufficient flexibility in device choice, these newer devices may be something worth investigating.
Thank you,
Brett