Part Number: TMS320F28374S
Tool/software: Code Composer Studio
In the attached screenshot, deltaSpeed, deltaSpeedLimit values can be shown in the expression window.
In the sw, in "If conition", even the deltaSpeed is less than the deltaSpeedLimit value but still break point is coming into inside the if condition. May I know the reason for it.
Is there any problem with the break point?
Current CCS version is : 6.1.0.00104