Part Number: TMS320F28069M
Hi team:
We use F28069m for motor control. The motor works normally when use lab06a (Rated speed, rated torque conditions).
But when we use lab09 for field weakening control and configure:
gMotorVars.Flag_enableSys = true
The motor began to shake and couldn't spin. The parameters of motor is copied from lab06a directly when using weak magnetic field control.
What's the matter, please? In principle, after the routine works properly on lab06a, should it work properly on lab09? The operation steps are exactly as per the manual.
Best regards