Other Parts Discussed in Thread: UNIFLASH, C2000WARE
Hello.
I have Piccolo Launchpad (F280049CPZS) . Accidentally I flashed Boot_ROM, now want to restore it.
I use Uniflash 5.0.0.2289 and F28004x_ROM.out from C2000Ware_1_00_06_00. Uniflash says:
[ERROR] C28xx_CPU1: File Loader: Verification failed: Values at address 0x3F9800@Program do not match Please verify target memory and memory map.
I also tried to recompile sources from C2000Ware v1.4, v1.5 and also v1.6 with v18.12.2 and v6.4.12 compilers, but I have the same error in CCS 8.3.
So is there way to flash LaunchPad Boot section?