This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: SPI Slave mode: SPISTE mandatory?

Part Number: TMS320F28377S


Hello

I start to design a board for Endat2.2 interface feedback.

I will us the same as presented into PM_Endat22_lib-SPRUI35.pdf

On chapter §1.5, a scheme indicat to set always the SPISTE to the Ground. BEcause into this schem, no need ChipSelect. Always activate it.

If I want get a GPIO for general purpose, Can I do not configre the GPIO27 as SPI? If no pin configured to the SPISTE function, isSLAVE SPI hardware will run correctly? (Is without any GPIO configured into SPISTE, the SPI slave module will consider the SPISTE always active?)

Thank