This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: Inverter recommendation

Part Number: TMS320F28374S

Hi,

Is there TIDA or C2000 recommendation for below inverter solution requirement?

1. DC30~60V input, AC220V output. above 90% efficiency.

2. It's better have mppt tracking function.

3. If hasn't total solution, solar inverter including software is also fine.