Hi E2E,
I am attempting to rebase a project from Motorware16 Lab20 to Motorware18 Lab11a and am having a slight issue. I have the migration complete but cannot reach any target RPM in Lab11a. The speed always falls about 85%-93% short of the speed reference target RPM. Another interesting data point is that my gMotorVars.Flux_VpHz variable in the updateGlobalVariables functions is also follows this trend of being slightly lower than I would expect.
Some info about my project:
- Custom hardware implementation
- Target Processor is TMS320F28027F.
- PWM Frequency is 10kHz.
- Target RPM is 19,000 RPM on a 4 pole PMSM. Ls is about 117uH, Rs is about 53mOhm, flux is 0.0437 V/Hz
- I am not intending on using RsRecalc, PowerWarp, RsOnline, Overmodulation or Field Weakening.
Does E2E have any insight into this issue?
Please let me know if I am missing any information that could help solve this and thanks in advance for any help!