Part Number: TMS320F28379D
Other Parts Discussed in Thread: SFRA, C2000WARE, POWERSUITE
Hi
I am using SFRA (this version C:\ti\c2000\C2000Ware_DigitalPower_SDK_1_03_00_00\libraries\sfra\gui).
I can get sweep result. when I open csv file in the compensation designer. I found compensation designer's bode plot(plant part) is not match with the csv file data.
for example :
my control ISR Freq is 20 Khz
plant bandwidth should be between 5565.19~6324.639 Hz(at -3db),if I using csv file to locate it.
compensation designer bode plot result is 1715Hz (at -3.105db)
Am I missing some setting?
csv file
Andrew