Part Number: TMS320LF2406A
Other Parts Discussed in Thread: SPRC074
Hi Champs,
>Some details to post are: Which link on this page is customer needing more information for JTAG, RS232, API, etc.? What is the error? Is this production >programming or field returns? The RS232 does have a download available for sprc074, is this the tool used?:
Customer created 10 boards. 1 board occurred flash error.
Customer is using sprc074 tool.
Error phenomenon is bellow
Exexcute this command and flash file.
serhost1.exe hs000.hex
<Error log>
BAUD rate detect .........
OK
Initializing device ...
Waiting.
OK
Clearing
Waiting..
OK <- Wrong ACK received. program terminated.(Failure board stopped at this command)
Erasing
Waiting...
OK
Programming
・
・
Could you please see any reason due to chip issue ?
Regadrs,
Kz777