Tool/software: Code Composer Studio
Hi TI experts,
I have implemented the single-phase SOGI PLL provided by TI. It works well. But I do not know which parameter should I use from the following structure in SPLL_1ph_SOGI_IQ.h, if I want to know the rms amplitude of a single-phase AC? I need this in order to detect possible grid under-voltage.
typedef struct{
int32 u[3]; // Ac Input
int32 osg_u[3];
int32 osg_qu[3];
int32 u_Q[2];
int32 u_D[2];
int32 ylf[2];
int32 fo; // output frequency of PLL
int32 fn; //nominal frequency
int32 theta[2];
int32 cos;
int32 sin;
int32 delta_T;
SPLL_1ph_SOGI_IQ_OSG_COEFF osg_coeff;
SPLL_1ph_SOGI_IQ_LPF_COEFF lpf_coeff;
}SPLL_1ph_SOGI_IQ;
Thank you in advance for your help!