This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSCNCD28M36: I cant find a file for loading on XDS100v2 USB Debug Probe_0/Cotrtex_M3_0

Part Number: TMDSCNCD28M36
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

testing example build is done taget ok but loading is not okay help me

  • SungJin,
    Note that this controlCARD has an isolated XDS100V2 on board. So plugging in the USB connection to the side of the controlCARD will power the emulator only(why you see target OK).

    You will need to supply power to the MCU from the docking station that it is plugged into(either with another USB cable or a 5V barrel connector).

    Please look at the InfoSheet here: C:\ti\c2000\C2000Ware_1_00_06_00\boards\controlCARDs\TMDSCNCD28M36\R1_1 to understand which LEDs indicate each domain has power.

    Best,
    Matthew
  • Thanks for your super kindness bro but Actually we got some miss points

    i supply power voltage in control card already actually i got customized PCB

    i know what you saying so you says i got just usb(minitype) powerconnections and loading connect so worrying about perfect operation the Card right?

    anyway i need 

    [XDS100v2 USB Debug Probe_0/Cotrtex_M3_0] file for load on my target(?)

    for make allowing for usb(not mini one for downloading) and LAN communications