This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28069M: Locked rotor test

Part Number: TMS320F28069M


Tool/software: Code Composer Studio

Hi,

Currently, I'm working on an 3 phase Induction motor drive which is rated at a peak power of 30kW. And if I want to use FAST algorithm for sensorless control, I need to do a locked rotor test. But, I don't have the equipment which can do that exercise. What am I missing here if I don't have data from locked rotor test? How does it affect the performance of the drive?

Thanks,

Harish K.