Part Number: TMS320F28335
Tool/software: TI-RTOS
Hello,
I am using CCSv9.0.1.00004
I done the following so far:
1. Installed XDCtools 3_51_03_28
2. Installed sys/bios 6_76_01_12
3. Created a CCS project
4. Created a new RTSC configuration file
When I double click on the configuration file, I get the error shown below. I noticed that the xdctool listed is 3.55.00.11 instead of 3.51.03.28 that I installed.
Please help me in setting up a RTOS project for C2000.
Stephen
js: "./config.bld", line 10: Error: Can't find the target named 'devkits.target.Generic' along the path 'C:/Users/sxxxx/workspace_v9_TestRTOS/TestRTOS/.config;C:/ti/ccs901/xdctools_3_55_00_11_core/packages;..;': please check the spelling of the target's name and that it exists along this path.
js: "./config.bld", line 10: Error: Can't find the target named 'devkits.target.Generic' along the path 'C:/Users/sxxxx/workspace_v9_TestRTOS/TestRTOS/.config;C:/ti/ccs901/xdctools_3_55_00_11_core/packages;..;': please check the spelling of the target's name and that it exists along this path.