Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Sir,
We are doing a project on the speed control of pmsm. We are following the ti document HVPM Sensored FOC of PMSM, but instead of using the HV Motor Control + PFC Kit, we are using tms320f28335 dsp board. The main confusion with the document is that the values are taken as in per unit form in all level builds, What is the main idea behind the calculation of these per unit values as we are using a pmsm motor with specifications of 300 VDC,16 A, 4000 RPM?