Part Number: TMDSHVMTRPFCKIT
Tool/software: Code Composer Studio
from Sensorless Field Oriented Control of 3-Phase Induction Motors on page 34, we have the real-time graph as shown below. from the graph, the horizontal axis indicates/says samples and the vertical axis has the variable value in per unit. i want to know the operating frequency of the waveforms, i do not get material on how to get the frequency from the real-time graph. but from the graph, i can observe the frequency is approximately 50Hz referring black line below. is this guess possible to know the frequency? if not how could i know it?