Hi Champs,
My customer is using F28069 and internal regulator to generate Vdd. They observed the Vdd on some device is higher than 1.9V which is very close to 1.995V max value. Thus, they worry the Vdd will become higher than max value under some circumstances and they want to know if this is a normal situation. On the datasheet, we only noted the voltage input range when using a external source. What is the normal measured Vdd range when internal regulator is used?
Thanks,
Brian