This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: TMS320F280049CPZS, WE NEED TUV OR UL CERTIFICATION FILES AND NUMBER.

Part Number: TMS320F280049C

Hi Sir,

TMS320F280049CPZS and TMS320F28377DWZT are designed on our board.

Our products is Solar Central Inverter, market cover all over the world.

We need TUV and UL certification files and certification number.  please help to provide. thanks.

Cyan,

Arrow

  • F28x7x has been certified by TUV for ASIL-B/SIL-2 hardware random compliance and ASIL-D/SIL-3 systematic capability compliance and the certificate is available at the following location:

    There is an IEC 60730 class C and UL 1998 class B compliant Safety Diagnostics Library (SDL) available for F28x7x

    All the requirements in Table H.1 of Annex H of the IEC 60730 Class C have been met by this SDL

     

    Access to this library may be requested by the system integrator

    There are no plans to get this SDL independently recognized by UL

    Plans for developing similar SafeTI enablers for F28004x are still being finalized. We will publish them once plans are final.

    This should address the question posed