Other Parts Discussed in Thread: CONTROLSUITE, SFRA
Tool/software: Code Composer Studio
Hi,
I'm working with a project based on the Dual Motor Control Using FCL example project in Controlsuite. All development this far has been made in the CCS debug mode with a RAM configuration. Now I would like to test it in stand alone mode meaning that load the program into Flash and run it in RAM. Thus I could boot in in standalone mode without the debugger. I don't want to execute any code from Flash.
Steps I have done:
1. Switch to flash mode: Build Configurations > Set Active > choose F2837x_Flash
2. Use the default linker cmd file that is given in the project files:
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
/* RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
*/
RAMLS3_4 : origin = 0x009800, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3_4, /* | RAMLS4, */
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3_4,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
/* The following section definitions are for SDFM examples */
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333
// DCL lib
dclfuncs : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)
/* SFRA test */
SFRA_F_Data : > RAMGS11, PAGE = 1
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
3. Build it succesfully.
4. Try to load it unsuccessfully and get the following error:
C28xx_CPU1: File Loader: Verification failed: Values at address 0x86000@Program do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\ti\controlSUITE\libs\app_libs\motor_control\libs\FCL_SFRA\v01_00_00_00\Examples\git_repo\FCL_28379D\F2837x_FLASH\FCL_379XL_git.out: a data verification error occurred, file load failed.
Any advise on how to solve this? I tried also other linker cmd files for F28379D that I found from Controlsuite but I get the same error. I'm using CCS8.