Part Number: TMS320F28069M
Hello,
I am using F2806X ISO-CONTROLCARD [R0.4] with USBDockingStation [R3], I am running BLDC motor of 60V, 250W attached with wheel for two wheeler application with sample code which is located here C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\BLDC_Sensored. I have my own driver card with driver IC IR2104S which is similar to DRV8312 as used in DRV8312EVM Rev D board. DFuncDesired is directly controlled by throttle.
Problem is initially there is a vibration in wheel then after it runs smooth. whether it is due to hardware or software?