This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternative to XE162/4 - Motor Control Forklift



Hi All,

I have a motor control application for forklift.

So far I was using XE164 (100pin) and XE162 (64pin). Now I want to re-design the whole board and adopt some changes and improve the technology in terms of performance, costs, reliability and safety.

Minimum requirements are:


- Asynchronous serial port (for programming and runtime configuration)
- CANBUS interface (minimum 2)
- Timer encoder interface with automatic forward-backward counting based on the fronts of the two encoder channels out of phase by a quarter of a period
- ADC: need to have two ADCs working internally at the same time
- PWM peripheral with double PWM piloting capability and timer (like CAPCOM Infineon): 2, one per type
- Clock at least 80MHz
- Minimum number of analog ports:
12 ports in the 100pin
8 ports in the 64pin

Proposals should be recommended for new developments, and with a long-term life perspective. (more than 10 years).

I look forward to any proposals.

Many Thanks,

Antonio