Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Dear All,
Thanks to TI, for you put Ethernet and EtherCAT interface to C2000. I have a few basic questions. It would be great if you answer.
- EtherCAT interface in the new TMS320F28388D is Slave Controller? Not master?
- One port Ethernet interface in the new TMS320F28388D is seen as IEEE 1588 supported. Could you a little explain the usage of IEEE 1588 in a control & automation work. I know that there is an master clock where shared the nodes over Ethernet. Say it is Precision Time Protocol. It is used to synchronize the many nodes over an Ethernet Network. What's the use of synchronizing all these nodes? Probably here is not correct forum this question, but it is important for new TMS320F28388D. Can you tell me the benefits of IEEE 1588 at the application level? (i.e: in a control & automation application) Can I use the IEEE 1588 for making the standard Ethernet to be deterministic & a 'level' of real-time? In the EtherCAT option, I need an EtherCAT master. However TMS320F28388D EtherCAT interface is probably slave controller? So, IEEE 1588 supported standard Ethernet might be better.
Thank you.