Part Number: TMS320F28379D
Tool/software: Code Composer Studio
I put most of my code int ramfunc to improve performance but in certain moment i had to extend the area form RAMLS4_LS5 to RAMLS3_LS4_LS5 then my code started to skip in to Interrupt_illegalOperationHandler. I have also checked to change. I have not understood the reason of such behavior so i have removed some of "__attribute__((ramfunc))" to fit my code to RAMLS4_LS5 and it works. I have also added the section RAMLS2_LS3 and replaced with RAMLS4_LS5. The program also skip to Interrupt_illegalOperationHandler. Could You please help to understand and find reason of such strange behavior. The code works properly only when i put into RAMLS4_LS5. There is my linker filter in the attachment.
// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMLS2_LS3 : origin = 0x009000, length = 0x001000
/*RAMLS2 : origin = 0x009000, length = 0x000800*/
/*RAMLS3 : origin = 0x009800, length = 0x000800*/
/*RAMLS4 : origin = 0x00A000, length = 0x000800*/
/*RAMLS5 : origin = 0x00A800, length = 0x000800*/
RAMLS4_LS5 : origin = 0x00A000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD0 : origin = 0x00B000, length = 0x000800
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAM_GS0_GS15 : origin = 0x00C000, length = 0x010000
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)
/* Allocate uninitalized data sections: */
.stack : > RAMD0 PAGE = 1
.ebss : {} RUN = RAM_GS0_GS15,
RUN_START(_start_ebss),
RUN_END(_end_ebss),
PAGE = 1, ALIGN(4)
.esysmem : > RAMD1 PAGE = 1
/* Initalized sections go in Flash */
.econst : > FLASHF PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.binit : > FLASHN, PAGE = 0 //ramfuncs copy info table
Filter_RegsFile : > RAM_GS0_GS15, PAGE = 1
DigitalPower : > RAM_GS0_GS15, PAGE = 1
SFRA_F_Data : > RAM_GS0_GS15, ALIGN = 64, PAGE = 1
SFRA_Data : > RAM_GS0_GS15, ALIGN = 64, PAGE=1
FPUmathTables : > RAM_GS0_GS15, PAGE =1
/* CLA specific sections */
Cla1Prog : LOAD = FLASHN,
RUN = RAMLS2_LS3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0, ALIGN(4)
CLADataLS0 : > RAMLS0, PAGE=1
CLADataLS1 : > RAMLS1, PAGE=1
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHN,
RUN = RAMLS2_LS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
{
--library=SFRA_F_Lib.lib<SFRA_F_INJECT.obj>
--library=SFRA_F_Lib.lib<SFRA_F_COLLECT.obj>
}
#else
ramfuncs : LOAD = FLASHN,
RUN = RAMLS2_LS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
{
--library=SFRA_F_Lib.lib<SFRA_F_INJECT.obj>
--library=SFRA_F_Lib.lib<SFRA_F_COLLECT.obj>
}
#endif
#endif
/* The following section definition are for SDFM examples */
#if 0
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
#endif
#ifdef CLA_C
/* CLA C compiler sections */
//
// Must be allocated to memory the CLA has write access to
//
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > RAMLS1, PAGE = 1
.scratchpad : > RAMLS1, PAGE = 1
.bss_cla : > RAMLS1, PAGE = 1
.const_cla : LOAD = FLASHB,
RUN = RAMLS1,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
PAGE = 1
#endif //CLA_C
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/