Other Parts Discussed in Thread: C2000WARE,
Tool/software: Code Composer Studio
Hello Experts,
I received some questions from our customers.
1. C2000WARE v02.00.00.02 Release Notes says,
there listed total 13 changed as the "Fixed in this release", then they picked up the following changes
which might related to TMS320F280049 device.
C2000DRIVERS-1939 F28004x CLA examples fail in Flash configuration S2-Major
C2000DRIVERS-1907 ADCINTFLG Workaround S1-Critical
C2000DRIVERS-1894 DCAN - some bit rates not working S3-Minor
C2000DRIVERS-1677 EPWM: EALLOW is not being used in APIs related to global reload functionality S2-Major
Are these changes really related to the TMS320F280049 device?
Do they need to move to C2000WARE v02.00.00.02 because of these changes?
Or can they stay on C2000 ware version 1.06.00.00?
2. SPRUI46B.pdf,C2000Ware Quick Start Guide describes as follows.
C2000Ware (v02.00.00.02) requires:
• CCS v9.0.1 or newer
• C2000 Compiler v18.12.1 LTS or newer
• ARM Compiler v18.12.1 LTS or newer
Can you explain the reason why they needs to upgrade to CC v9.0.1 from their current version 7.3?
3. If they need to change the version from 1.06.00.00→2.00.00.02.
Are there any procedure document to change the version?
Especially, they think they need to change the driverlib file, so these related documets are expected.
Regards,
A.Fujinaka