This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: UNINITIALIZED SECTION GETTING INITIALIZED

I am using Code composer studio Version: 8.1.0.00011 , for development of part No : F28379D .
In my application i want to use a global variable which is not initialized during watchdog reset .

For that i have declared a variable like this

#pragma DATA_SECTION(resetreq_ecust,".shared");
uint16_t resetreq_ecust;

And in Linker command file i have added in section like this

.shared : type = NOINIT, run = 0x604 , PAGE =1

In my code i have implemented some logic like , for 60 seconds watchdog will refresh and after that it will stop refreshing , because of which in every

60 seconds , watch dog will cause MCU reset . But at the start of main only , I am writing value 0x5A5A to resetreq_ecust .

After writing i checked resetreq_ecust is holding 0x5A5A value .

But after 60 seconds when watchdog causes reset , resetreq_ecust value becomes 0 , i.e it get initialized .
In map file i have also checked , shared location is uninitialized

.shared 1 00000604 0000000a UNINITIALIZED
00000604 0000000a ecum.obj (.shared)

and

resetreq_ecust is located at same location :

address data page name
-------- ---------------- ----
00000400 10 (00000400) __stack

00000604 18 (00000600) _resetreq_ecust

But not able to figure out why variable is getting initialized .

I have attached linker and map files as attachemnt , any help will be appreciated .linker_and _mapfiles.rar