This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Increase rafunc size

Part Number: TMS320F28069M


Hi TI community,

I would increase the ramfunc size on a TMS320F28069M to fit 2 interrupts inside. 

The current size (RAML0 + RAML1) is not enough. (code : RAML0_1     : origin = 0x008000, length = 0x000C00 and 

ramfuncs : LOAD = FLASH_D_H,
RUN = RAML0_1,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0

I tried to increase the size while using RAML2 and RAML3. But it does not work (they are not on the same page). (code RAML0_3     : origin = 0x008000, length = 0x800 + 2 * 0x400 + 0x1000 and 

ramfuncs : LOAD = FLASH_D_H,
RUN = RAML0_3,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0

How can I do ?

Many thanks