Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Here are a few questions regarding VCU0 CRC support on F28004x.
1. Regarding the function getCRC32_vcu(): Is the polynomial fixed as POLYNOMIAL32 0x04c11db7, or can this be changed?
2. How exactly can the reflected table be used? In the docs, this is implied, but it is not clear. In general, is there any additional documentation which can shed some light?
3. There could be an issue with the code. It seems that when set to Even Parity, it functions correctly, but there may be an issue with Odd Parity... Is there a working example for Odd Parity? Can this operation be verified?
4. When will we have F28004x VCU0 CRC examples in C2000ware? I think this would help out greatly.
Thanks,
Eric