This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: TMS320F28035 can wake up hard ware

Part Number: TMS320F28035

On-board (OBC) uses DSP, 28035 master control. Is there any reference design about can wake-up related hardware circuit?

  • I presume you are referring to the low-power mode wake-up using the CAN module. Is this correct? If so, you need to determine which one of the 3 low-power modes (IDLE, STANDBY or HALT) your system will be using. This would determine what wake-up signal would bring the device out of the low-power mode. There is no special H/W requirement for the wake-up circuit. The wake-up process is handled in S/W.