I am using launchpad's 3.3v for 5.5Kohm potentiometer, MPL3115A2_Altitude pressure sensor .
First time I had directly connected 3.3V supply to POT (5.5Kohm) from launcher and output of pot is directly connected to ADCINB2 / ANALOGIN pin.
Immediately after starting debug 3.3V and GND are partially shorted (resistance between these two is 31ohm) and ADCINB2 / ANALOGIN pin and 3.3V got shorted.
Then i kept one 470ohm resister in series with 3.3V and POT then its working fine.
yesterday i have initialized one more ADC pin ADCINA3 / ANALOGIN for my appicatiion. when i started debugging it got damaged .ADCINA3 / ANALOGIN is reading continuously 256 adc value .
I don't understand why is this happening. Why 3.3V and GND are getting shorted and one of the ADC pin is damaging ?
And one more question SMA-J-P-H-ST-EM1 is not present on Launchpad ? what is the use of it ?