Part Number: TMDSHVMTRPFCKIT
Tool/software: TI C/C++ Compiler
Dear TI Hello,
I am working on the HVACI control project,
In the HVACI_Sensorless_2833x project, current As and Bs are measured and normalized,
// Measure phase currents, subtract the offset and normalize from (-0.5,+0.5) to (-1,+1).
// Connect inputs of the CLARKE module and call the clarke transformation macro
Could someone tell me please for which current value the (-1,+1) correspond?
Does it correspond to the base current defined in the project [1=>10A]?
Thank you in advance,
S.Tarik,