This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1000: tidm1000

Part Number: TIDM-1000
Other Parts Discussed in Thread: UCD3138, UCD7138

Regarding LLC  design in the TIDUCT9 document, the output interleaved connection seems to be wrongly printed. A typo?

From TIDUCT9–January 2017 document, can you comment to this observation pl: in the attached document in pdf?tidm-1001 system_output.pdf

r

  • can the code used in TIDUCT9–January 2017 LLC interleaved design using C2000 be ported to or reused in UCD3138 ...hopefully with minimum changes?

    We are using UCD 3138 in many products under development & with UCD7138 chips...so it will be of great help in time-to-market for our version of ultracompact 5V /400W Interleaved design if we could.

    thnx for any help in this matter.

    robin 

  • 1. There is no path for the code to run on UCD3138 as it is designed for C2000. This will be an exercise you will need to take for your development. 

    2. The doc has a issue , you are correct the connection should not be there. I will file this as a bug and have it fixed.