This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/SM320F2812: Debugging on TMS320F2812 vs SM320F2812

Part Number: SM320F2812

Tool/software: Code Composer Studio

Good Afternoon, 

We have been debugging/integrating on an eval board, ezdsptms320f2812 without issue and have recently switched to our tactical hardware which uses the SM320F2812HFGM150.  We are receiving warnings related to unconfigured memory.   It appears to flash the device successfully, however, it doesn't not appear to run properly.  

We have verified the XCLKIN and XCLKOUT are running 30MHz and 150Mhz respectively which indicates that it has run through the PLL setups and our initialization functions.   In addition, the watchdog is not asserting as we would expect.  Also, if we try to force a watchdog assertion, it is ignored. 

Is this anything we need to be aware of with the differences in parts that would cause these behaviors outside of the pinout and packaging differences?

Vr, Dan